DUG_Multiwire Puck Dimmer_WH–03

About the device

The Wiser Multiwire Micro Module LED Dimmer (hereinafter referred to as Dimmer / Micromodule Dimmer) combines the advantages of smart dimmer functionality with ordinary mechanical push-button switches. It transforms a conventional switch into a connected device which can be controlled by a push button or through the Wiser app. It can switch and dim the ohmic or capacitive loads and it is also compatible with dimmable LEDs.
NOTE: Do not control any devices that depend on a permanent power supply.

Additional features:

  • Remote control with maximum of 10 single mechanical push-buttons.

  • Setting the LED operating mode manually (RL LED mode).

  • Electronic overload protection, overheating protection, and short-circuit protection.

  • Setting the dimming range: minimum and maximum brightness.

  • Setting a time schedule with the Wiser app.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?