DUG_PowerTag-E_WH-09

Automation

An automation allows you to group multiple actions that are usually done together, triggered automatically or at scheduled times when certain conditions are met. Using the Wiser Home app, you can create automations based on your needs.Automation is applicable only for users with EV Charger and Wiser hub installed together. An automation allows you to group multiple actions that are usually done together, triggered automatically or at scheduled times. By using the Wiser Home app, you can create automations based on your needs.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?