Creating an automation
-
On the Home page, tap
.
-
Tap Automation
>
to create an automation.
-
Tap
and choose an icon that best represents your automation.
-
Enter a name of the automation (A) and select any of the
following conditions to meet (B).
- All conditions: All conditions must be met to trigger an automation
- Any condition: Any one of the condition must be met to trigger an automation.
-
Tap Add conditions (C) and select
any of the following (D):
- Device status change (Select the device)
- Away Mode (Enable or Disable)
NOTE: Maximum 10 conditions can be added. - Select a device (E) that will set the condition.
- Drag the sliding bar up/down to open/close the shutter or adjust the position as per need. Example shutter in Open or Closed state.
- Tap Set.
-
To add an action, tap Then > Add an action and select any of the following (F):
- Control a device: Select a device that you want to trigger.
- Send notification: Turn on the notification for the automation.
- Activate a moment: Select the moment that you want to trigger.
NOTE:-
Maximum 10 actions can be added.
-
You can add one action in an automation; to add another action, you must create another automation.
- Select Main hall light (G) device and set an action on/off.
- Tap Set.
-
Tap Save.
The saved Automation is displayed on the Automation page. Tap the toggle switch to enable/disable the Automation.