DUG_Smoke alarm DC_WH-01

Pairing the device

Using the Wiser Home app, pair your device with the Wiser Hub.
IMPORTANT: Do not mount the device before pairing. The Setup/Reset button and power switch are located on the rear side of the device.
NOTE: When multiple smoke alarms are paired with the same Wiser Hub, an 868MHz radio frequency (RF) interconnection is automatically created between smoke alarms.
To pair the device:
  1. Locate the power switch on the rear side of the device. Use a screwdriver to turn the power switch to ON position.

    NOTE: When the device is mounted on a wall or on the ceiling, the power switch is automatically turned ON.
  2. On the Home page, tap .
  3. Tap Devices > > Safety and Security .
  4. Tap Smoke Alarm > Next .
    The next screen shows the progress of the pairing.
  5. Short press the Setup/Reset button 3 times.

    The LED blinks yellow.
  6. After a few seconds, a solid green LED indicates that the device is successfully paired and the app shows that the device has joined.

  7. Tap Next to assign a name to the device.
  8. Tap Next to assign a device location and then tap Submit.
    TIP: The device is now listed under the All devices or room tab.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?