DUG_Smoke alarm DC_WH-05

About the device

The Wiser Smoke Alarm – Battery (smoke alarm) uses a photoelectric sensor to detect smoke generated by fire. It also includes a temperature sensor that detects heat caused by rapid increase in temperature. When connected to the system the device sends the notifications via the Wiser app.

Operating elements

  1. Status LED (Amber, Green and Red LED)

  2. Standby LED (Red LED)

  3. Test/Hush button

  4. Power switch

  5. Setup/Reset button

Installation location

  • Smoke Alarm can be installed on a flat/inclined ceiling, or on the wall.

  • Do not install smoke alarms near windows, doors, or ducts.

  • Avoid paint, stickers, or other decorations.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.