DUG_Smoke alarm DC_WH-04

Maintenance and cleaning

A monthly inspection is recommended to help ensure the smoke alarm is dust, dirt, and insect free. The smoke alarm can be vacuumed (strongly recommended) or brushed with a soft brush to remove accumulated dust, dirt or kitchen grease. Apply a small amount of insect surface spray to a cloth and wipe around smoke alarm(s) every 3 to 6 months to mitigate insect ingress.

IMPORTANT:
  1. Always test the smoke alarm after cleaning, for more information refer testing the device.

  2. If necessary refer to the installation instruction for more information about installing the smoke alarm.


NOTICE
EQUIPMENT MAINTENANCE INSTRUCTIONS
  • Test the smoke alarm regularly to ensure its functionality and the battery is in good condition.
  • Replace the smoke alarm after 10 years from the date of manufacturing.
  • Do not open the smoke alarm casing or repair yourself. There are no serviceable parts inside.
Failure to follow these instructions can result in equipment damage.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.