DUG_Smoke alarm DC_WH-05

Testing the interconnected device(s)

It is possible to test all the smoke alarms simultaneously in an interconnected network with one operation.
  1. Select any interconnected device.
  2. Press and hold the Test/Hush button for more than 10 s until an alarm goes off on all interconnected devices.

  3. If there is no alarm triggered on the interconnected smoke alarms, check if the distance between each smoke alarm is within the specification. Also check that the smoke alarm is On and working properly. Refer troubleshooting smoke alarm battery.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.