DUG_Multiwire Puck Dimmer_WH–01

Pairing the device

Using the Wiser Home app, pair your dimmer with the Wiser Hub to access and control the dimmer.
  1. On the Home page, tap > Devices > > Lights > Micromodule Dimmer > Next
    NOTE: The next screen shows the joining process of dimmer.
  2. Select any of the following:
    • Short press the Set (setup/reset) button 3 times (<0,5 s) on the dimmer with a screwdriver.
    • Short press the mechanical push button (wired to terminal 1 of the dimmer) for 3 times.
    The LED blinks amber.
    NOTE: If the dimmer is located behind the push button, the status LED is not visible.
  3. Wait for a few seconds until the LED turns green. You can also see in the app that the device is joined.
    After a few seconds, a solid green LED indicates that the device is successfully paired to the Hub.

    NOTE: If the LED is blinking green and red, see the instructions by tapping the link LED not blinking amber? .
  4. Tap , to enter the name of the device.
  5. Tap Next and assign the device to a new room or an existing room and tap Submit.
    IMPORTANT: The next screen shows the Device Settings page, where you have the option to configure the device settings during the pairing process or at a later time. If you prefer to configure it later, tap Submit. For more information on device settings, refer to Configuring the device section.
    The dimmer is now listed under All devices.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?