DUG_Micro Module Light Switch_WH-04

Setting up a schedule

The devices can be fully controlled by schedule. Once the schedule is set, the devices operates at a given time.
To create a schedule:
  1. On the Home page, tap .
  2. Go to Schedules > to create a schedule.
  3. Enter the name of the schedule (A).
  4. In the TYPE menu, select Lights (B).
  5. In the APPLIES TO menu, select Micromodule Switch (C) from the listed devices.
  6. Tap Create to setup events.
  7. Tap to add an event such as STATE (lights on/off) and WHEN ( sunrise/sunset or specific time range).
    NOTE: Tap to copy the schedule from one day to other days or copy the entire schedule to a new schedule or to an existing one, which will overwrite it.
  8. Tap Set to save the schedule.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?