DUG_Smoke alarm DC_WH-04

Testing the individual device

IMPORTANT:
  • Test the smoke alarm once a month to ensure proper operation.

  • If the smoke alarm is installed in a mobile home, test weekly and before every journey.

Press the Test/Hush button on each smoke alarm for more than 3 s until an alarm goes off. If the alarm does not go off, either the battery is low or there may be other technical issues. Refer troubleshooting smoke alarm battery.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?