UG_Wiser Home Essential API_WH-00

About the Wiser Home Essential API

The Wiser Home Essential API (hereinafter referred to as API) is designed to facilitate seamless integration and control of various home automation systems. This API allows software developers to manage and interact with Wiser Home hubs and their functions such as:

  • Heating

  • Lighting

  • Electrical Loads

  • Sensors

  • Shutters

It provides a secure and standardized way to communicate with the Wiser Home system, facilitating smart and sustainable home solutions for professionals managing multiple homes in shared residences.

Using this API, you can create custom workflows based on the building manager’s requirements for the existing system. Once you create the workflows or energy dashboards, the building manager can access it and monitor/control the devices.

NOTE: The use of this API is restricted to qualified software engineers only. Improper use may lead to system vulnerabilities or data integrity issues. Ensure that you have the necessary expertise before accessing or utilizing this API.

IMPORTANT: You must subscribe to the Wiser Home Essential API before you can use it. Once subscribed, you can see the API credentials in the Exchange portal > Wiser Home Essential API > View Credentials.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.