UG_Wiser Home Essential API_WH-00

Fetching the Hub Details by URN

You can fetch hub details such as ID, product type, device lock status, and signal strength using the Try It section.
IMPORTANT: You can find this urn ID when you fetch the list of hubs.

Prerequisites

Before you start, ensure you have the following details:

  • API Subscription Key

  • Bearer Token

  • urn ID

  1. On the left pane, click Hubs.
  2. Click Fetch Hub by URN.
    The API window appears.
  3. On the right pane, click Try It.
  4. In the Security (A) section, enter the following details:
    • API Subscription key (B): Enter the subscription key.

    • Bearer token (C): Enter the bearer token.

    NOTE: Your credentials will be saved until the end of the browser session.
  5. In the Parameters section, enter the urn ID (D).
  6. Click Send (E).
You can see the hub details.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.