UG_Wiser Home Essential API_WH-00

Fetching the Awaymode Status

You can check whether the hub status is in Awaymode (ON or OFF).

Prerequisites:

Before you start, ensure you have the following details:

  • API Subscription Key

  • Bearer Token

  • urn ID

  1. On the left pane, click Hubs.
  2. Click Fetch Awaymode Status.
    The API window appears.
  3. On the right pane, click Try It.
  4. In the Security (A) section, enter the following details:
    • API Subscription key (B): Enter the subscription key.

    • Bearer token (C): Enter the bearer token.

    NOTE: Your credentials will be saved until the end of the browser session.
  5. In the Parameters section, enter the urn ID (D).
  6. Click Send (E).
The hub status will be displayed. If the status is true, Awaymode is ON. If the status is false, Awaymode is OFF.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.