UG_Wiser Home Essential API_WH-00

Fetching the List of Devices

You can fetch the list of devices in the Wiser System using Try It section in the API. Here is an example of fetching the list of smartplugs. You can follow the same process for all devices to fetch the list of devices.

Prerequisites:

Before you start, ensure you have the following details:

  • API Subscription Key

  • Bearer Token

  • urn ID

  1. On the left pane, click Control.
  2. Click List Smartplug.
    The API window appears.
  3. On the right pane, click Try It.
  4. In the Security (A) section, enter the following details:
    • API Subscription key (B): Enter the subscription key.

    • Bearer token (C): Enter the bearer token.

    NOTE: Your credentials will be saved until the end of the browser session.
  5. In the Parameters section, enter the urn ID (D).
  6. Click Send (E).
You can see the list of Wiser plugs.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?