UG_Wiser Home Essential API_WH-00

Examples of API Functions

Using the Try It section in the API, you can perform the following actions:

Here is the Try It section screen:

  • The hub urn (Unique Reference Number) ID is required to fetch the list of commissioned devices.

  • Both the hub urn ID and the device ID are required to control the devices.

The following topics are examples of fetching a list of hubs and hub details.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?