UG_Wiser Home Essential API_WH-00

Using Developer Documentation to Access API Functions

You can find the documentation on the Wiser Home Essential API development portal. This is the main source of truth for developers to check the regular updates and API versions. The documentation explains features such as:

  • Hubs

  • Control

  • Heating

  • Sensors

  • Energy

  • Equipment

Authorization Model

Once the building manager subscribed to the Wiser Home Essential API, they can create a Personal Access Token (Bearer Token) and share it with the developer to access the API or add the developer to the Developer Group to grant API access. You can see the Subscription key in Wiser Home Essential API > View Credentials > Credentials.

Developers need a Subscription Key and a Personal Access Token (Bearer Token) to access the API and perform integrations.

To create a PAT, refer to the Creating a Personal Access Token for more information. You can see the PAT in Wiser Home Essential API > PAT.

Downloading the API

You can download the API in different formats such as JSON and YAML from the Exchange portal.

To download:

  1. Click Wiser Home Essential API.

  2. On the Wiser Home Essential API page, click Select Format.

  3. Select your preferred format from the dropdown menu:

    • JSON

    • YAML

    NOTE: The Download button will be enabled once you select the format.

  4. Click Download.

    The API will be downloaded in the selected format.

Once you download the API, you can use several tools to work with it.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.