UG_Wiser Home Essential API_WH-00

Controlling the Devices

You can control devices, such as turning it ON/OFF, adjusting the shutter percentage, setting the light brightness, and setting the temperature. Refer to the Turning ON/OFF the Device topic. You can follow the same process for all devices by changing the body field based on the device type.

In the Body field of the Try It section, enter the following details based on the device you want to operate:

Device

String

Lights and Dimmers

On/Off and percentage

Shutters

Percentage

Energy

On/Off

Heating

Degree centigrade

Sensors

On/Off

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.