Creating an automation
- On the Home screen, tap
.
- Go to Automation >
to create an automation.
BEMÆRK: Maximum 10 automations can be added. - Tap If (A) and select any of the
following conditions (B):
- All conditions: This triggers an action only when all conditions are met.
- Any condition: This triggers an action when at least one condition is met.
- Tap Add conditions and select any
of the following (C):
- Device status change: Select a device to enable automation.
- Away Mode: Enable/Disable away mode
to trigger an action.
TIP: Away mode can also be used as a trigger to turn off the lights, dimmer or closing the shutter etc. For more information about Away Mode, refer to the system user guide.
- Tap Device status change > Temperature/Humidity Sensor > Temperature. Set the temperature using sliding bar (D) and select the condition (E) (less than / more than), then tap Set.
- To set a specific time for your automation, tap When > Add time and select any
of the following (F):
- Specific time of the day: Sunrise, Sunset, Custom.
- Period of time: Daytime, Night time, Custom.
- To add an action, tap Then > Add an action and select any of the following (G):
- Control a device: Select a devices that you want to trigger.
- Send notification: Turn on the notification for the automation.
- Activate a moment: Select the moment that you want to trigger.
-
Wait: This option allows you to add a delay in an automation sequence. You can set the wait time in increments of 1 hour and 1 minute, up to a maximum of 24 hours. This feature is useful for delaying actions within an automation.
- Tap Control a device > Heating and select any of the following (H):
- Boost: Set the duration to increase the temperature by 2° C.
- Setpoint: Set the desired temperature.
- Tap Setpoint, set the required temperature using vertical sliding bar (I), then tap Set.
- Enter the automation name (J).
- Tap Save.
Once the automation is saved, it is visible on the Automation tab.