DUG_Temperature/Humidity Sensor_WH-07

LED indications

Pairing

User Action

LED Indication

Status

Press the function key 3 times

LED blinks amber, once per second.

Pairing mode is active for 30 seconds. When pairing is completed, LED glows green for some time before turning Off.

Resetting

User Action

LED Indication

Status

Press the function key 3 times and long press once for > 10 s.

After 10 s, the LED starts blinking red.

The sensor is in reset mode. It is reset to the factory settings after 10 seconds. The sensor then restarts, and the LED starts blinking green before turning Off.

Battery level

LED Indication

Status

LED blinks amber once per minute.

The battery is low (< 10 %), replace the battery.

NOTE: A notification pop-up will appear on the app.

Identifying the device

LED Indication

Status

LED blinks green.

 Sensor is connected to the Wiser Hub.

NOTE: This function is initiated from the app to identify the sensor.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?