DUG_Temperature/Humidity Sensor_WH-07

Using the device

The Control Panel of the sensor allows you to view the real-time temperature and humidity values.
  1. On the Control tab, tap All devices or a room tab where the sensor is located.

  2. On the sensor control panel page, you can see the following:

    • The current temperature value (A)

    • The current humidity value (B)

    • History (C)

    • Device settings (D)

    • Add to favourites (E)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?