DUG_Temperature/Humidity Sensor_WH-07

Setting the device as temperature source

You can configure the Temperature/Humidity Sensor as the primary device for measuring room temperature. The temperature readings from the sensor will be used as an input for controlling the heating system. If the room has multiple temperature measuring devices such as the Wiser Room Thermostat, Connected Flush-mounted thermostat, or Temperature/Humidity Sensor, the system automatically calculates the average temperature from all devices. This ensures that heating is regulated based on a more accurate overall room temperature.
IMPORTANT: This option is only available if you have installed any one of the following Wiser heating device:
  1. On the Home screen, tap .
  2. Tap Devices > Temperature/Humidity Sensor.
  3. On the Device Details page, turn on the toggle switch to enable temperature/humidity sensor as a temperature input source.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?