DUG_Temperature/Humidity Sensor_WH-07

Pairing the device with the Wiser Hub

Using the Wiser Home app, you can pair your sensor with the Wiser Hub.
  1. On the Home screen, tap .
  2. Tap Devices > >Climate > Temperature/Humidity Sensor.
    TIP: You can also navigate by tapping Control > > Climate > Temperature/Humidity Sensor.
  3. Tap Scan QR code and allow the Wiser Home app to access your camera. Then, scan the QR code located on the device.
    NOTE: If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4.

    If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options:

    • (A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI–64 and Install code are valid.

    • (B): Tap this option if you are unable to find the Mac Address/EUI–64 and Install code.

  4. Tap Next, short press the function key 3 times and make sure that the LED blinks amber.

    Wait for a few seconds until the LED turns green and the app confirms that the sensor is joined.
  5. Ensure that the first battery cover is securely fastened, then install the sensor on the base plate. For more information, refer to the installation instruction.
  6. Tap , to enter the name of the sensor.
    NOTE: If you are already using any of the following Wiser Heating devices, then proceed to Step 8. If you wish to use the Temperature/Humidity Sensor for temperature control in conjunction with a heating device, then proceed to Step 7.
    • Wiser 16 A Relay for Temperature Control

    • Wiser Radiator Thermostat

    • Wiser Underfloor Heating Connection Strip

  7. Turn on the toggle to allow the Temperature/Humidity Sensor to measure room temperature in conjunction with your thermostat.
    TIP: When this feature is enabled, temperature reading from the sensor and the thermostat are combined. This ensures a more accurate representation of room temperature and helps optimize heating control.
  8. Tap Next and assign the sensor to a new room or an existing room and tap Submit.
    IMPORTANT: The next screen shows the Device Settings page, where you have the option to configure the settings during the pairing process or at a later time. If you prefer to configure it later, tap Submit. For more information on device settings, refer to Configuring the device section.

    After you pair the device, a success screen appears with the following options:

    • + Add New Device: Tap to continue pairing more devices.

    • Start Using Your Device: Tap to start using the paired device.

    NOTE: The success screen appears only if you are logged in as a Home Owner.

    Now, you can see the newly added sensor on the Control tab under the All and Room tabs.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?