DUG_Temperature/Humidity Sensor_WH-07

About the device

The Wiser Temperature/Humidity sensor (hereinafter referred to as sensor) combines two sensors in one unit. The sensor measures temperature and humidity in the environment where the sensor is installed. When the sensor is connected to the Wiser Hub, it reports the temperature and humidity data to the Wiser Hub.

The sensor triggers other Wiser devices (such as turning on an air conditioner if the temperature is high or turning on an exhaust fan if the humidity is high) through automation.

Features of the sensor:

  • Detect temperature and humidity in the environment and passes the information to the Wiser Hub.

  • Sends the battery level and offline device status information to the Wiser Hub.

Operating elements

  1. Status LED

  2. Function key

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?