DUG_Temperature/Humidity Sensor_WH-07

Replacing the battery

  1. Remove the sensor from the base plate by sliding it upwards.
  2. Unscrew the battery cover using a screwdriver.
  3. Replace the battery with the proper polarity.
  4. Re-install the battery cover and tighten the screw using a screwdriver.
    The LED blinks green seven times and then stops blinking.
  5. Install the sensor on the base plate by sliding it down.
    NOTE: Dispose used batteries, as per statutory regulations.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?