DUG_PTC_WHP-01

About the device

PowerTag Control (PTC) is a wireless-communication module explicitly designed for controlling and monitoring applications. It is part of PowerTag System and Wiser System, turning a distribution board into a connected panel.

PowerTag Control can monitor a circuit and notify the Wiser Hub wirelessly of the status of a contact (OF, SD, CT, or TL position indication).

PowerTag Control monitors circuits wirelessly, collecting status of daisy-chained circuit breakers and notifying the Wiser Hub of information status, such as OFF, Contactor (CT) or Impulse Relay (TL) position indication. The PTC has a volt free relay contact providing control of 230 VAC loads up to 2 A.

  • Zigbee technology simplifies cabling and commissioning operations: no wiring is required for the PowerTag Control modules to communicate with the Wiser Hub.

  • System scalability: PowerTag Control modules can be easily installed in new or existing panels at any time with a simple commissioning operation.

  • PowerTag Control modules are DIN rail mounted.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?