DUG_PTC_WHP-01

Editing a schedule

You can edit an existing schedule according to you preference.
  1. On the Home page, tap Automations .
  2. Tap the schedule you want to edit.
  3. Tap the SCHEDULE DETAILS and you can do the following actions:
    • Rename the schedule (A).
    • Within the Applies to (B) menu, you have the option to select from the listed devices or deselect those that are already selected.
    • Under the EVENTS (C) menu, you can edit the day and then tap to edit an event such as STATE (On/Off) and WHEN (specific time range).

    NOTE: When the above changes are edited, the schedule is saved automatically.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?