Configuring the device
-
Tap (or the room where PowerTag is assigned) and select the device which you want to configure
|
A |
Zigbee Signal Strength Indicator: Zigbee Signal Strength indicator which displays the current signal strength of the device. |
|
B |
Type: Tap to change the label according to your preference. TIP: You can also select Custom option at the end of list and select a custom
label.
|
|
C |
Device Name: Tap to change the name of the device. |
|
D |
Location: Tap to assign the Device to any room (such as living room, bedroom, kitchen etc). Refer to setting the device location for more details on how to set the location. |
|
E |
Advanced settings: Tap to change the Output type and wiring condition, Refer advanced settings. |
|
F |
Identify: Tap to identify the device. The status LED blinks red and connected
lighting devices blinks On/Off, upon successful identification of
the dimmer. |
|
G |
Delete: Tap to remove the device from the system. NOTE:
|