DUG_PTC_WHP-01

Switching On/Off the device using app

Using the Wiser Home app, you can switch on/off the device.

On the Home page, tap the power button to switch on/off the respective device

Alternatively, you can navigate to the control panel of the device and tap label to switch on/off the device.

NOTE: The control panel shows the current state of the device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?