DUG_PTC_WHP-01

Creating an automation

  1. On the Home page, tap Automations .
  2. Go to Automation and then tap to create an automation.
  3. Enter a name of the automation (A) and select any of the following conditions to trigger an automation.
    • All conditions:: All conditions must be met to trigger an automation
    • Any condition: : Any one of the condition must be met to trigger an automation.
    TIP: You can choose the cover image that represents your automation by tapping
  4. Tap Add conditions (B) and select any of the following (C):
    • Device status change (Select the device): An automation will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor.
    • Away Mode (Enable or Disable): The Away Mode is intended to set your Home to a practical state for longer absences, such as leaving for the weekend.
    NOTE: Maximum 10 conditions can be added.
  5. Select a device to set the condition. Then, choose the state of the device that will trigger the automation, such as the On/Off state.

  6. Tap Set on the upper right corner.
    TIP: If you want to change the condition, swipe it to the left and tap the bin icon. Then add a new condition with the required parameters.
  7. To start your automation at a particular time, tap When > Add time and select any of the following (D):
    NOTE: Maximum 10 time entries can be added.
    • Specific time of day:The automation will trigger at a specific time of the day, such as at sunrise, sunset, or at 8:00 AM.
    • Period of time:The automation will be trigger during time periods such as from sunrise to sunset, from sunset to sunrise, or from 8:00 AM to 5:00 PM.
  8. To add an action, tap Then > Add an action and select any of the following (E):
    NOTE: Maximum 10 actions can be added.
    • Control a device: Select the device and set the desired state of the device.
    • Send notification: You will be notified if the condition is met.
    • Activate a moment: Select a Moment.
    • Wait: This option allows you to add a delay in an automation sequence. You can set the wait time in increments of 1 hour and 1 minute, up to a maximum of 24 hours. This feature is useful for delaying actions within an automation.
  9. Tap Control a device and select the required device to preform the action tap Set located on the upper right corner.
  10. After setting all condition and action, tap Save.
The saved automation is displayed on the Automation page. Tap the toggle switch on the automation to enable/disable it.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?