DUG_PTC_WHP-01

Using the device

The Control Panel allows you to switch the device On and Off and control various settings.

On the Home page, tap on the device icon to open control panel page.

On the control panel page, you can see the following:

  1. Switch to turn on/off the device.

  2. Current state of the device.

  3. Create or assign a schedule

  4. Device setting to change the configuration.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?