DUG_PTC_WHP-01

LED patterns

Behavior

Communication indicator light

PowerTag switched off.

PowerTag is searching for a Hub in pairing mode.

PowerTag is in identification mode.

PowerTag is in network. Normal communication with the Hub.

Occasional loss of communication.

Loss of communication with the Hub.

Internal error detected.

Firmware upgrade in progress.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?