DUG_1 Channel Relay Puck-00

Adding a Device to the Room

You can add a device to a room using the Wiser app.

To add:

  1. On the Home screen, tap Devices > Rooms.
  2. Select the room from the list.
  3. Tap + (A) to add a device.
    TIP: If no devices are assigned to the room, tap > + to add a device from the Add Device screen.
  4. Select a device from the Add Device screen. Refer to pairing the device with the Wiser Hub topic of the respective device user guide for the next steps.
    TIP: When you turn the room ON/OFF (B), the devices that have been added to that room are activated.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.