DUG_1 Channel Relay Puck-00

Editing a trigger

To edit a trigger:

  1. On the Automation screen, tap Trigger.
  2. On the top-right screen, tap .
    The Edit Actions List screen appears.
  3. On the Edit Actions List screen, tap the trigger you want to edit.
    TIP: If you want the same trigger, tap the hand symbol, it will copy the same trigger and add it to the Edit Actions List.
  4. You can perform the following changes:
    • Change the icon.

    • Rename the trigger.

    • Add a device or an action.

    • Add a trigger.

    • Remove a device or an action.

    • Remove a trigger

  5. Once all edits are done, tap Update.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.