DUG_1 Channel Relay Puck-00

Renaming a room

You can rename a room using the Wiser app.

To rename:

  1. On the Home screen, tap Devices > Rooms.
  2. Select a room from the list.
  3. On the top-right screen, tap .
  4. Enter a new name in the room name (A) field.
    TIP: Tap on the device that you want to remove from the room.
  5. Tap Done (B).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.