DUG_1 Channel Relay Puck-00

Changing the Wi-Fi access point

You can change the Wi-Fi network using the Wiser app.
  1. On the Devices page, tap Devices.
  2. Select the device.
  3. Tap Settings > Device Details.
  4. Tap Change Access Point (A) to change the Wi-Fi network.
  5. Select the Wi-Fi network.
    TIP: If you can’t find your Wi-Fi network, try tapping Refresh (B). If you still cannot find it, you can manually enter the SSID by tapping Enter SSID (C).
  6. Enter the new Wi-Fi password in the password field (D).
    NOTE: The Connect button will be enabled after entering the password.
  7. Tap Confirm (E).
  8. Alternatively, you can also change the Wi-Fi access point manually by pressing the push reset power button 8 times in 10 seconds4 times in 10 seconds.

    If the puck is inside the wall, you can toggle the external connected switch 8 times in 10 s to change access point mode.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.