DUG_1 Channel Relay Puck-00

Technical data

Operating Voltage

 

100 - 240 VAC

Frequency

 

50/60 Hz

Max current

 

16 A

Max load

 

3000 W (Resistive)

Note: Widely supports most of the home appliances like Geyser, AC, Refrigerator, LED and fluorescent lamps etc.

Subject to Power factor.

Standby power

 

< 2.5 W (When the device is in Station Mode and when connected to a Wi-Fi® network)

Under voltage protection

 

< 90 Vac (Soft cut-off)

Over load protection

 

> 300 VAC (Soft cut-off)

Thermal Protection

 

Yes

Over temperature protection

 

Yes

Sustained surge protection

 

Yes

Energy monitoring

 

Yes

Wireless Frequency

 

Wi-fi (2.4 GHz)

Network range

 

Upto 30 m

Colour

 

White

Temperature

 

Operating: 0° C to 50° C

Storage: -20° C to 70° C

Relative humidity

 

10% to 95%

Compliance

Radio/RF

 

ETSI EN 300 328

Communication interface

 

Wi-Fi®: 2.4 GHz only, IEEE

802.11 b/g/n

Mechanical

Dimensions (L x W x H)

 

55.3 x 48.5 x 17.6 mm

Colour

 

White

Wire cross section

 

2.5 mm²

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.