DUG_1 Channel Relay Puck-00

Using the device

The Control Panel allows you to switch on/ off and control various settings.
On the Devices page, tap Devices and select the device to access the control panel.

The control panel displays the following options:

  • Schedule: You can schedule the ON time and OFF time of the device (A).

  • Energy: Displays the energy usage of the device (B).

  • History: Displays the history of usage of the device (C).

  • The current state of the device (D).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.