DUG_4 Channel Automation Relay-00

Configuring the device

Using the Wiser app, you can configure the device according to your preference.

  1. On the Home screen, tap Devices > Devices.

  2. Select the device from the list.

  3. On the Device Control Screen, tap .

    The Device Settings screen appears.

A

Device Name

Displays the device name, tap to change the device name. For more information, refer to the Renaming the device topic.

B

Change Room

Displays the assigned room of the device, tap Change Room to assign any room (such as living room, bedroom, kitchen, etc.). For more information, refer to the Changing the device location topic.

C

Radio Type

Displays the Z-Wave network.

D

Device Type

Displays the device type.

E

Signal Strength

Displays the signal strength.

F

Advanced Settings

Allows you to set group switches and configuration. When you tap Advanced Settings, you can see the following options:

  • Group Switches: Manage multiple switches as a single group.

  • Associate with other powered Z-Wave devices: Link your device with other Z-Wave devices for synchronized operation.

  • Group Association: Create associations between devices for coordinated actions.

  • View Configuration: Check the current settings and configurations of your device.

  • Set Configuration: Adjust and customize the settings of your device.

G

Product Details

Displays the product details such as manufacturer name, ID, product name, ID, and type. Also you can view the firmware version and update it if a new version is available by tapping Product Details > Firmware Version & OTA.

H

Notification

Enable the Notify Me toggle button to receive device notifications.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.