DUG_4 Channel Automation Relay-00

Pairing the device with the Wiser Hub

Using the Wiser app, you can pair your 4 channel relay puck with the Wiser Hub to access and control the relay switches.
  1. On the Home screen, tap Devices.
    The Device Management screen appears.
  2. Tap Devices > +.
    The Add Device screen appears.
  3. Tap Preferred > With Hub > 4 Channel Relay (A).
    TIP: You can also tap All > Switches and Controls > Z-Wave Switches and Controls > 4 Channel Relay .
  4. Enter the following Device Information and then tap Next:
    • Enter Device Name: Enter the device name.

    • Assign Existing Room: Select an existing room.

      TIP: If your room is not in the existing room list, create a new one.
    • Add New Room: Create a new room.

  5. Tap Next and choose one of the following options to pair the device with the Wiser Hub.
    • Press the pairing button once and make sure that the LED blinks green.

      Wait for a few seconds until the LED turns green.

      TIP: If the LED is blinking red, then the device is not paired to the Hub. Reset the device and start pairing again.
    • Press the toggle Switch-1 3 times (Sequence: ON-OFF ON-OFF ON-OFF) within 4 seconds.

      NOTE: If the relay puck is installed inside the wall box, the status LED is not visible.
  6. After a few minutes, you can see the Wiser message. Tap Ok.
    You can see the newly added device on the Device Management screen under Devices.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.