DUG_4 Channel Automation Relay-00

Using the device

The Device Control Screen allows you to switch ON/OFF the device and control various settings.
  1. On the Home screen, tap Devices > Devices.

  2. Select the device which you want to access the Device Control Screen.

The Device Control Screen displays the following options:

A

Power Button

Allows you to change the status of the device ON/OFF.

B

Schedule

Allows you to create quick actions and trigger automations.

C

History

Allows you to see the history of the device. Tap to update the history of the device when you open the History screen.

D

Settings

Allows you to control various settings. For more information, refer to the Configuring the device topic.

E

Favourites

Allows you to add the device to the favourites on the Home screen.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.