DUG_4 Channel Automation Relay-00

LED indication

Pairing the device

User Action

LED Indication

Status

Short press the programming button once.

Both red and green LED’s glows constantly.

Pairing mode is active. When pairing is completed, LED blinks green continuously.

Resetting the device

User Action

LED Indication

Status

Short press and hold the programming button for <10 s.

LED blinks red once per second.

The device is in reset mode. The device then restarts indicating that the device is ready for pairing.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.