DUG_Wiser Fan Speed Controller-00

About the device

The Wiser Fan speed controller is a miniature micro module (hereinafter referred to as Puck), which is remotely controlled and designed to operate in AC mains. This device enables 4/5 step fan speed control. The fan speed is controlled by mobile app or fan regulator. The puck also operates as a repeater within the Z-Wave network it is associated, and uses the latest Z-Wave plus chip.

  • 4-Step Fan regulator/5-Step Fan regulator

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?