DUG_Wiser Fan Speed Controller-00

Pairing the device with the Wiser Hub

Using the Wiser app, you can pair your fan controller puck with the Wiser Hub to access and control the fan.
  1. On the Home screen, tap Devices.
    The Device Management screen appears.
  2. Tap Devices > +.
    The Add Device screen appears.
  3. Tap Preferred > With Hub > Fan Controller (A).
    TIP: You can also tap All > Switches and Controls > Z-Wave Switches and Controls > Fan Controller.
  4. Enter the following Device Information and then tap Next:
    • Enter Device Name: Enter the device name.

    • Assign Existing Room: Select an existing room.

      TIP: If your room is not in the existing room list, create a new one.
    • Add New Room: Create a new room.

  5. Tap Next and choose one of the following options to pair the device with the Wiser Hub.
    • Press the pairing button once and make sure that the LED blinks green.

      Wait for a few seconds until the LED turns green.

      TIP: If the LED is blinking red, then the device is not paired to the Hub. Reset the device and start pairing again.
    • Press the toggle Switch-1 3 times (Sequence: ON-OFF ON-OFF ON-OFF) within 4 seconds.

      NOTE: If the puck is installed inside the wall box, the status LED is not visible.
  6. After a few minutes, you can see the Wiser message. Tap Ok.
    You can see the newly added device on the Device Management screen under Devices.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?