DUG_Wiser Fan Speed Controller-00

Add favourites

You can add your devices and automations to favourites for quick and easy control from the Home screen.

To add favourites:

  1. On the Home screen, tap.
    The Edit Favourites screen appears.
  2. Tap the icon to add all your favourite devices and automations.
  3. Once selected, tap Save.
    Now you can view all your favourite devices/automations on the Home screen.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?