Using the device
-
Select the device which you want to access the Device Control Screen.
The Device Control Screen displays the following options:
|
A |
Power Button |
Allows you to change the status of the device ON/OFF. |
|
B |
Speed Control |
Allows you to adjust the fan speed as per your needs by tapping 1, 2, 3, 4, or 5.
NOTE: You can see the 5 options (1, 2, 3, 4,
5) when configured with the 5-step fan speed regulator. If configured
with the 4-step fan speed regulator, you will see 4 options (1, 2,
3, 4) to control the speed.
|
|
C |
Schedule |
Allows you to create quick actions and trigger automations. |
|
D |
History |
Allows you to see the history of the
device. Tap |
|
E |
Settings |
Allows you to control various settings. For more information, refer to the Configuring the device topic. |
|
F |
Favourites |
Allows you to add the device to the favourites on the Home screen. |