Configuring the device
-
Select the device from the list.
-
On the Device Control Screen, tap
.
The Device Settings screen appears.
|
A |
Device Name |
Displays the device name, tap |
|
B |
Change Room |
Displays the assigned room of the device, tap Change Room to assign any room (such as living room, bedroom, kitchen, etc.). For more information, refer to the Changing the device location topic. |
|
C |
Radio Type |
Displays the Z-Wave network. |
|
D |
Device Type |
Displays the device type. |
|
E |
Signal Strength |
Displays the signal strength. |
|
F |
Change Fan Speed |
Allows you to adjust fan speed using the 4/5-speed regulator. For more details, refer to the Changing the fan speed regulator topic. |
|
G |
Advanced Settings |
Allows you to set configuration. When you tap Advanced Settings, you can see the following options:
|
|
H |
Product Details |
Displays the product details such as manufacturer name, ID, product name, ID, and type. Also you can view the firmware version and update it if a new version is available by tapping Product Details > Firmware Version & OTA. |
|
J |
Notification |
Enable the Notify Me toggle button to receive device notifications. |