DUG_Wiser Fan Speed Controller-00

Resetting the device

You can reset the device to factory default manually.

For resetting the micro module:
  1. Press and hold the Programming button for <10 s.
  2. After 10 s, the LED starts blinking red, and then release the programming button.
NOTE: All configuration data, user data, and network data are deleted. After which
  • No connectivity to other devices or rooms.

  • No moment or schedule settings.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?