DUG_Wiser Fan Speed Controller-00

Changing the device location

You can change the device location using the Wiser app.

To change the device location:

  1. On the Home screen, tap Devices > Devices.
  2. Select the device for which you wish to change the location.
  3. On the top-right screen, tap .
    The Device Settings screen appears.
  4. Tap Change Room (A).
  5. Select the desired room from the list (B).
    TIP: If your room name is not present in the list, you can create a new room by tapping the + (C) button.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?