DUG_Wiser Fan Speed Controller-00

Switching ON/OFF the device using the app

Using the Wiser app, you can switch ON/OFF the device.

To switch the device ON/OFF:

  1. On the Home screen, tap Devices > Devices.
  2. Find the device you want to switch ON/OFF.
  3. Tap (A) to turn ON/OFF the device.
  4. On the Device Control Screen, tap the power button to turn the device ON/OFF (B). Select the fan speed by tapping the control options 1, 2, 3, 4, or 5 (C).
    TIP: You can also turn the device ON/OFF when you add it to your Favourites. To know more about Favourites, refer to the Add Favourites topic.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?