DUG_Wiser Fan Speed Controller-00

Changing the fan speed regulator

You can change the fan speed regulator to a 4-step or 5-step using the Wiser app.
IMPORTANT: You must change the fan regulator manually to either a 4-step or 5-step before proceeding to the following steps.

To change:

  1. On the Home screen, tap Devices > Devices.
  2. Select the Fan Controller device.
    The Device Control Screen appears.
  3. On the top-right screen, tap .
    The Device Settings screen appears.
  4. Tap Change Fan Speed.
  5. Select one of the following fan speed types:
    • 4 Fan Speed Regulator

    • 5 Fan Speed Regulator

  6. Change your fan speed regulator to speed 1 and then tap Next.
  7. Change your fan speed regulator to speed 2 and then tap Next.
  8. Change your fan speed regulator to speed 3 and then tap Next.
  9. Change your fan speed regulator to speed 4 and then tap Next.
    TIP: For a 5-step fan regulator, you need to change your fan speed regulator to speed 5 and then tap Next.
    You have successfully changed the fan speed regulator.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?